“readychain®” for machining center
“We have been using pre-assembled energy supply systems for over a year on a turning and grinding machine,” says Oliver Fechner. This concerns a high speed finishing center for turning, grinding and polishing rotogravure cylinders, the 'Finishing Center CFM Compact'. The unit can be integrated with automatic production lines. It is used in the package printing sector. “We are setting standards in our industry with this finishing center,” adds Christoph Gschoßmann. Seven energy supply systems in total are used in the small series, of which two are pre-assembled “readychains®”. Six move the axes, one the control cabinet. “For the die carrier, we rely on the readychain® from the start. The speed of the tool shaft is about 9 m/min, the travel distance at about 2.5 m. Due to the positive experiences, we decided as the next step to also equip the movable control panel with the pre-assembled version,” says Oliver Fechner. “And our long-term objective is to have all six axes delivered as a complete mechanical subassembly to install on the finishing center ready for use. ” The energy supply system from Series 39 is used. This design represents the standard on chains of this size. The series offers the best compromise between ease of assembly, stability and costs for nearly all application areas. It is distinguished among other things by a dual stop system, is corrosion resistant and suitable for tight installation conditions. Even with long travel distances, a high unsupported length is achieved with this chain. “The enclosed chain design is used incidentally on the control panel, in order to protect the cables from chips, for example,” adds the mechanical engineer, Stephan Bobritz. “All other energy supply systems on the other hand are protected in the machine housing!” The pre-assembled energy supply system is made up of at least 150 individual parts: cable types, hoses, connectors, contacts, inscriptions. Among others, “chainflex®” cables prove their all-round ability as highly bending-resistant control, encoder and converter cables. “As this finishing center involves a small series, we were able to produce the configuration with a reasonable outlay in this case. From our point of view now sells itself. The effort involved in ordering is much less for our purchase department. We only have to specify the order number now and get the pre-assembled energy supply system delivered on time for installation,” says Stephan Bobritz pointing out the economic benefits.