"The world has never seen a stadium like this," enthused FIFA President Joseph Blatter about the VELTINS Arena at Gelsenkirchen. The European football association UEFA classified the multifunctional stadium as a 'five-star stadium' of the top-most class: "The venue more than meets the requirements and could even be rated as a 'six-star stadium'." One of their hallmarks is the mobile playing field. It is moved over a single distance of 170m with the help of two space-saving
roller energy chains and special cables from igus® GmbH in Cologne.
From Bruce Springsteen to State summit meetings
These hymns of praise underscore the resonance the arena has received since its commissioning in August of 2001. It quickly established itself as one of the continent's most advanced event venues. UEFA classified the stadium into the highest classification 4. Millions of people have until now not only attended athletic events. The bandwidth ranges from stock car races to music concerts and biathlons.
The stadium is completely financed with private sector funds and compels with its technology. The mobile grass field, the retractable roof, the sliding south bleachers, and the giant video cube under the roof are only some of the technical highlights. The "Knappenkarte" has been established as a cashless payment system based on a chip card. The tickets are also based on chip technology and provide smooth and reliable access control.
Oversized tray as drawer: the mobile field
The playing field of the VELTINS arena is more than green grass. Bedded onto a 118 m long and 79 m wide tray, it is the only mobile lawn within the Bundesliga, and can travel back and forth for a distance of approx. 340 m. It was modeled after the Gelredome in Arnhem (Netherlands).
The grass surface is essentially only in the stadium during games. The exterior storage ensures ideal conditions for the sensitive grass surface. The stadium bleachers are high and generally prevent direct sun irradiation. This noticeably affects the lawn, which would otherwise need to be replaced every few months with expensive sod“, explains Michael Blaß, Sales Manager for energy chains and other products at igus® GmbH in Cologne. "And our roller energy chain is used for the power supply to move the field. They require very little room and have demonstrated their strength from the beginning. “
The principles behind the mobile playing field are relatively straight-forward. The 11,000 tonne tray is inserted into and retracted from the arena just like a drawer. 16 steel rails were integrated into secondary floor, the foundation, to ensure that this works smoothly. Each rail is 25 cm wide and 300 m long. The tray with the lawn is transferred into the arena on these.
The field is moved by four hydraulic presses, so-called gripper jacks. The presses move the playing field forward at one-and-a-half metres per minute. The motor then releases itself from its anchor, advances the ram on the steel rails in the secondary floor, clamps back down and re-engages. The entire process lasts 3.5 to 4 hours.
Roller energy chains: rolling instead of gliding
The roller energy chain, rol-e-chain®, is predestined for applications in which long travels are executed at high speeds. This is the case for instance in photo-finish cameras or in materials handling systems. Savings can be achieved even in slower applications in the crane sector or in shunting facilities due to the low friction coefficients of the system, as the drives can be dimensioned considerably smaller.