Solution
All the above crane systems are equipped with two or three harnessed energy supply systems from igus for longitudinal and transverse travel. One is the
energy chain system E4.1, which can be opened from both sides, and is very robust and protects the inserted cables.
Not only in material handling, but also in the erector, which is responsible for placing the tubbing, robust energy supply systems prove their strength. For the tubbing segment lining, immediately after the drilling process, the tunnel is supported permanently with the tubbings in the form of a ring to protect the shield skin. The tubbing segments are positioned on the tunnel wall by means of an erector, a remote manipulator, held mechanically or by vacuum, and then screwed. The erector's radius of action of +/-200° is achieved with
energy supply systems of the E4/4 series with reverse bend radius (RBR) and an installation position turned by 90°.
E4/4 chains are characterised by high stability and torsional strength. They can be opened from both sides and equipped with various mounting brackets. Long unsupported applications, also mounted on the side, are implemented just as reliably as gliding applications. The e-chain series proves itself especially in harsh environmental conditions.
In addition, a harnessing with bending-resistant chainflex signal and high-voltage cables from igus was carried out.