Four-fold increase in load capacity
Multi-dimensionally moving energy supply system for a palletising robot
This energy supply system easily moves in all axis and reliably guides cables even with difficult geometries. This distiguishes it from corrugated hoses, which do not hold up over the long term when exposed to pronounced rotating motions. Expensive equipment downtime is the result. A German company relies on a universal module for all robot motions on its palletizing robot in a fully automated packaging line. The solution guarantees a long service life and reliability.
"We have rigorously relied on robot technology for our packaging plants for about 20 years", reports Michael Ruf, procurator and Deputy General Manager at Transnova-RUF Verpackungs- und Palettiertechnik GmbH in Ansbach (Central Franconia). They are each tailored to the respective customer application. Each year, we integrate more than 200 robots into our plants", states Michael Ruf. "They give our customers a maximum of flexibility for the final packaging process. “
Compact universal module
A foil packaging plant that is delivered as a turnkey facility now uses a compact triflex® RS universal module made by igus® GmbH, Cologne, for the palletising robot. The module ensures that the energy chain is always guided closely to the robot to avoid loops and unnecessary cable stresses. It is assembled on the existing mounting points on the robot and consists of a triflex® R multi-axis energy supply system, model 'easy', version B (TRE 60.B). The series is predestined for fast insertion of the various cables. Version B also provides an improved connection mechanism and increased stability, therefore resulting in further improvements of machinery or plant availability.
Limit stop dogs also ensure a defined mobility limit, therefore providing additional protection. The system also uses integrated fibre rods to reliably guide the energy chain and a cover system. This is a cover that holds the energy supply system in place when the robot operates in a vertical or overhead orientation.
Efficient and reliable packaging
With its approx. 220 employees, transnova-RUF supplies solutions for final packaging and palletising tasks, ranging from planning to design-engineering, assembly and commissioning. The product range includes individual compact machines for top and side loading, picking systems for fast pick&place applications, and robot systems for order picking, palletising, and depalletising tasks, and even fully customised final packaging lines.
"We are equipped to handle any type of primary packaging", Michael Rug explains. "This ranges from button batteries for hearing aids to complete control cabinets with a length of 2.20 m. " Ranging from food and non-food applications to medical or pharmaceutical technology: the specialist has flexible packaging solutions for any industry. The company has been growing in double-digits for years. 75 percent of its customers are located in Germany. And 90 percent of these are repeat customers. They are expanding existing plants or rely on the specialist for new investments.
Flexibility due to robotic palletising.
"Our robot palletising technology is principally characterised by high flexibility and a maximum of reliability", the procurator clarifies. Modular function groups allow handling of cartons, buckets, bags, plastic buffers, etc. The picking tools are capable of handling a wide range of pallets and intermediate layers.
In total, a foil packaging plant has a length of 60 m. Each foil roll is dedicated to a customer-specific order. Each foil roll can have a different length and/or thickness, and a resulting difference in weight. The foil material itself also differs. The various foil rolls are fed to the packaging plant in a chaotic manner and need to be flexibly handled based on the sequenced production orders. "This task is predestined for robot technology", explains Michael Ruf. "A total of nine robots are in use. “
The packaging process consists of the following steps: after production, the foils travel from cardboard rollers into the plant. Here, they are staged in a buffer or sorting station before they are subsequently coated with a protective hose-foil. The hose-bag protrusion is blown into the roll core with compressed air. The primary packaging unit has now been packaged and is then individually packaged, labeled, and sealed. The product is then palletised on two pallets by a long-arm robot. A top stretch winding secures the two respective pallet packaging units.
"The packaging plant will be operated 24/7", Michael Ruf underscores the requirement profile. The respective packaging weight ranges between 2 kg and 60 kg. The conveyor technology speed is approx. 40 m/min. 20 rolls per minute can be packaged.