Solution
Due to the combination of climatic and mechanical demands that would have arisen on the high seas, a conventional metal chain was not an option for the energy supply.
Instead, an
e-chain of the E4/4 series from our energy chain portfolio is travelling here today. It protects the
chainflex motor and signal cables, also provided by us, during the turbine's lifting and lowering movements along a travel of 20 metres. During this process, the robust energy chain is guided in a steel trough.The vertical lifting movement is converted into a horizontal one via a 90° deflection. And the most important thing in this application: the plastic chain eliminates the need for any maintenance on the open sea, which made it the only solution considered by the operators.