Normal bus cables cannot be used due to their inherent weight. Their lack of a carrying member means that they can only bear loads up to 15 N/mm². Taken together, all these facts mean that the freely suspended cable could be over 1 kilometre long before having to contend with any decrease in performance. "For us, this means that we could theoretically increase the height of the building significantly," states the construction organisation manager. Initially, an additional cable was installed in the lift system to provide an added safety margin to be on the safe side and to make it possible to measure the data records that were generated. The lift systems are used very frequently. Just under six months after the system was commissioned, it had already made some 56,970 trips. After two years, they will have easily surpassed a figure of 160,000 without any hint of a malfunction. "The system is certainly not going to reach the maximum number of trips for which it is certified. A new lift control system will be installed first well before that," says igus sales advisor Eugen Kowalczyk with confidence. On the other hand, chainflex® cables for industrial applications are designed for very small bend radii, high numbers of cycles, high speeds, high accelerations and demanding environmental conditions.