Special ambient conditions for energy chains
The mobile scraper at the primary clarifier, which travels along a gantry above the primary clarifier, needs several minutes each time to convey oils, fats and the settled sludge to the end of the tank, where it is pumped off and fed to the treatment plant. Here, the axes do not run at one-second intervals. Despite the low speed, however, this is not a "low-end" application for movable cable guides. On the contrary, the energy supply system must function all year round and outdoors in 24/7 operation - in frost, strong sunlight, in corrosive, sometimes aggressive environments and with minimum maintenance.