While the requirements in the area of material handling, especially intralogistics, are increasing continuously, the demands placed on the materials used due to the goods to be transported are also rising. Given the increasing speed, one important element of drive systems must always function reliably: the bearing. There are different types of guide roller: driven guide rollers made of steel, types made of stainless steel or plastic. They are used to establish a rolling contact between the conveyor frame and the conveyor belt. The guide rollers supplied by igus® can be used flexibly and, depending on the requirements, can be fitted with different deep groove bearing bearings. The igus® conveyor rollers are not only used in the area of material handling but also in labelling machines, the packaging industry and the food industry, where they are sometimes used as guide rollers.
Visit the shop