Solution
According to these specifications, igus first developed a movable cable only with thermocouples, which is now included in the product ranges as
chainflex CFTHERMO. K.001, as well as a cable with three copper wires and a thermocouple (CFTHERMO. K.002). The cable type K.002 was tested at igus and MS Spaichingen and the MS designers issued the approval after 300,000 double strokes. In the meantime the CF thermo cables have been in use for some years, and the experience is all-round positive. Joachim Wein, in charge of Electronics Development for the Welding Technology Business Unit at MS Spaichingen: "We use the cables with and without energy chains and haven't had a single failure yet."
igus has expanded the CFTHERMO product range and added further alloys that are used, for example, for measuring higher temperatures. Moreover, since last year the
readycable harnessed cables for thermocouples, have been available. The connectors are made of the same material as the cables. The dynamic tests that igus carried out with the first chainflex thermal cables are, still reliable. They started in January 2011 and have now reached over 100 million double strokes, and the resistance measurements still show no irregularities. In the meantime, igus has also encountered other applications for such cables - even in-house, more precisely in the injection moulding plant, where several hundred injection moulding machines produce plain bearings, energy chains and other igus products. In these machines, the temperature of the process must also be monitored, and this task is undertaken by thermocouples. Also, increasingly more movable cables are used in other areas, which have the properties of a thermocouple and at the same time are extremely reliable.