Solution
The developers chose igus energy chains for safe guidance of hoses and cables. In total, there are 25 energy chains in the system. In addition to 19
E4.1 e-chains, MSG Production AS installed six
2400 series energy supply systems. The material igumid G ensures that the chains are insensitive to moisture and chemicals. Even temperatures down to -40 degrees Celsius are no problem. Both energy chains are dirt-resistant and do not require lubrication, making them ideal for use in de-icing or cleaning equipment.In cable guidance, igus products are also used for mounting nozzles. igubal pillow block bearings reliably ensure mobility for individual nozzles. Their position on the floor and the bars also permanently exposes them to chemicals and moisture. Like all products from the motion plastics specialist igus, the bearings are lubrication-free, corrosion-free, wear-resistant and have low-friction. Another advantage is that the service life of the bearings and e-chains can be calculated quickly and easily with
online tools. The forecasts are based on more than 12,000 tribological tests and 10 billion test cycles a year in the company's own 2,750-square-metre test lab. This gives customers reliable information about the service life of the bearings, e-chains and cables they use and helps avoid unplanned system downtimes.