Please choose your delivery location

The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Contact
igus® Ltd.

Caswell Road

Northampton, NN4 7PW

01604 677240
GB(EN)

igubal® pillow block bearings


igubal® pillow block bearings are up to 40% more cost-effective and up to 80% lighter than comparable metal solutions. Their operation is also more economical, because they are lubrication-free and therefore maintenance-free.

igubal® pillow block bearings have a high level of durability and stiffness – even when they are exposed to demanding ambient conditions over years. They are resistant to media, corrosion-free and function properly even in liquids and media. Even UV radiation from the sun, nuclear radiation and temperatures between -30 and +80°C do not have any negative impact on their running properties and their wear resistance.

The pillow block bearings are additionally resistant to dust and dirt. The pillow blocks are available for shaft diameters from 5 to 50mm (tolerance: h6 to h9).
The spherical balls provide automatic angle compensation. This enables the bearings to automatically equal out alignment errors and edge loads, misalignments and deflections of the shaft. In contrast to bearings made of metal, they are also able to absorb and dampen high-frequency vibrations.

 

Contact an expert

igubal® pillow block options

KSTM pillow block bearing

KSTM pillow block bearings
  • Dimensional series: K following DIN ISO 12240
  • Housing material: igumid G 
  • Material of spherical ball: iglidur® W300
  • Very high durability in varying loads
Visit the shop

ESTM pillow block bearing

ESTM pillow block bearing
  • Dimensional series: E following DIN ISO 12240
  • Housing material: igumid G 
  • Material of spherical ball: iglidur® W300
  • High radial loads
Visit the shop

ESTM-SL, slim line pillow block

KSTM-SL
  • Extremely lightweight
  • Extremely space-saving
  • With M3 thread or hole for self-tapping screws
  • Spherical ball material: iglidur® J
Visit the shop

ESTM-FC, FDA compliant pillow block bearing

ESTM FC pillow block
  • Housing material: igumid FC180
  • Material of spherical ball: iglidur® FC
  • Made of FDA-compliant materials
  • detectable 
Visit the shop

Pillow blocks made from sheet metal, PP204

JEM pillow block bearing
  • PP204 up to PP208
  • Lubrication-free and maintenance-free
  • Cost-effective
  • Resistant to dirt
Visit the shop

ESQM, Split pillow block for sqaure profiles

square profile pillow block
  • Profile 100, 110, 120 or 140mm
  • Split version of housing and spherical balls
  • Easy assembly and disassembly
  • High loads
Visit the shop

When to use it?

When chemical resistance is required

When a low-cost alternative is desired

When dirt-resistant bearings are needed

When misalignments should be compensated

When fully split components are needed

When not to use?

When temperatures above +80°C prevail

When an integrated collar is required

When dimensions over 50 mm are needed

When rotation speeds in excess of 0,5 m/s should be implemented


Successfully in use by our customers

ESQM pillow block bearing application

Reliable tracking with igubal pillow block bearings

To ensure that solar unit daily tracking movement works perfectly, the company uses our robust igubal ESQM pillow block bearings – a "fit and forget" solution, since they are maintenance-free throughout their 25-year service life.
Pillow block bearing application

Pillow block bearings in a catamaran

Recreative Electric Vehicles, a shipyard in southern France, is building an electric catamaran that is 80% recyclable. Since weight is crucial, the company installed our lightweight plastic pillow block bearings, which require no maintenance or lubrication.

Shop!

I am familiar with igus® products and would like to see the selection of pillow block bearings in the online shop or immediately place an order.
Visit the shop

Information

I need more information on variants of pillow block bearings or would like to know what the advantages of pillow block bearings from igus® are.
Send an enquiry

Consulting

I would be happy to answer your questions

Photo
Alan Hicks

Business Unit Leader for Fast Growing Products

Write e-mail

Shipping and consultation

In person:

Monday to Friday from 8am - 8pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH